Modbus RTU Supported Devices
The Modbus RTU Communications option supports communications to the following programmable controllers:
- Series Six with CCM3 card (Version 1.06 or later)
- 3720 ACM Electronic Power Meter (Firmware Version 1.5 or later is required if you want to read/write negative numbers)
- Modicon 484
- Modicon 584
- Modicon 884
- Modicon 984
- Modicon Micro 80
- Generic PLC - This is a special device model for generic devices where the user defines the device characteristics.
- DYN_PLC - This is a special device model for generic devices. The range of each of the memory types is determined by the device communication interface.
- STAT_PLC - This is a special device model for generic devices where the user defines the device characteristics and starting addresses for points are validated by reading them from the device.