Toggle Between Data Update Modes
About this task
Normally, domain data is only read when the domain display is initiated or when you click on the Read from PLC or Write to PLC buttons.
todo:
To update data automatically:
Procedure
- Click on the File menu.
-
Select Live Update from the submenu.
Result: When Live Update is enabled, the domain values are read and updated automatically approximately every 3 seconds.
todo: To return to manual mode: - Click the File menu. Note that Live Update has a check mark next to it.
- Select Live Update again to turn off the Live Update mode.