Modbus RTU Hardware Installation
Procedure
- Configure the controller/communications card for Modbus RTU communications.
- Assign each server within the configuration a unique server address between 1 and 247 (decimal).
-
Configure all servers at the same baud rate and parity as the client (the Modbus RTU Communications enabler).
Connecting to a Series Six
To connect a personal computer to a Series Six with a CCM3 card installed, refer to the Series Six Programmable Controllers Data Communications Manual (GFK-25364).