OPC UA Client Device
About this task
OPC UA device configuration enables you to:
- Configure the connection to the UA server.
- Define a user identity that will be associated with the UA Session.
- Add/modify subscriptions and common configurable items available to CIMPLICITY.
- OPC UA Device: New
- OPC UA Device: Configure
OPC UA Device: New
CIMPLICITY provides many ways to open a New Port dialog box.
Procedure
- Select Devices in the Workbench left-pane.
-
Do any of the following.
- Double click Devices.
- Right-click Devices; select New on the Popup menu.
- Click File>New>Object on the Workbench menu bar.
- Click the New Object button on the Workbench toolbar.
- Press Ctrl+N on the keyboard.
A New Device dialog box opens when you use any method.
-
Enter/select the following
Device Name for the OPC UA Client device. Port An OPC UA Client port from the drop down list of configured ports. - Click OK.
Results
The Device dialog box opens.
OPC UA Device: Configure
1 | OPC UA Client Device: General Tab |
2 | OPC UA Client Device: OPC UA DA Configuration Tab |