Alarm Management API Contents
The following is a list of all files distributed with the Alarm Management API. The files are loaded into the directories indicated. The environment variable %BSM_ROOT% is the directory where the CIMPLICITY software was installed.
Include files in %BSM_ROOT%\api\include\inc_path are:
alarmapi.h | cor_thread.h |
am_defs.h | cor_time.h |
am_errors.h | ddl.h |
amap_defs.h | examgr.h |
amaru_err.h | ipc.hpp |
amdd_cmd.h | ipcerr.h |
amdd_cont.h | mf_defs.h |
amdd_defs.h | mfamupdi.h |
amip.h | mfpmterm.h |
cor.h | mfstatus.h |
cor_event.h | netcom.h |
cor_mutex.h | rcm.h |
cor_os.h | rtr_bcst.h |
cor_stat.h | sc_recs.h |
Source files in %BSM_ROOT%\api\am_api are:
amaru_demo.c | makefile amaru_demo_exe.vcxproj |
Source files in %BSM_ROOT%\api\lib are:
amaru.lib | fasrtl.lib |
amip.lib | ipc.lib |
corutil.lib | cim_mf.lib |
ddl.lib | cim_sc.lib |
examgr.lib |