Error Messages
If the VALUE or RAW_VALUE field displays "******", there is a problem reading the point data from the device.
If a field displays "#N/A", the attribute you requested does not contain a value.
If a field displays "#NAME?", you can have one of several problems; for example:
- You have entered an invalid Point ID or attribute name.
- The attribute is not supported by the point type.
- CWSERV does not support the point type for value displays.
When you see a "#NAME?" error in a field, check your project's Status Log file for detailed information on the cause of the problem.