Login/Logout API Support
Several APIs exist that give programmed applications some control over the CIMPLICITY login/logout activities. Versions exist in both C callable and basicscript callable forms.
C callable routines
The C callable routines located in rcm.dll are:
COR_I4 GEFCIMPLICITY_setuserpw (TCHAR *proj, TCHAR *CIMPuser, TCHAR *pw)
COR_I4 GEFCIMPLICITY_remuserpw (TCHAR *proj, TCHAR *CIMPuser, TCHAR *pw)
COR_I4 GEFCIMPLICITY_login(TCHAR *proj)
COR_I4 GEFCIMPLICITY_logout(TCHAR *proj)
Be aware that:
- These functions are defined in the header file <inc_path\cor_user_api.h>
- To use these API's link with rcm.lib.
- The return value can be one of the following.
- COR_SUCCESS
- COR_WARNING
- COR_FAILURE
Corresponding basic script extensions
CimSetProjectUserPassword(CIMPuser as string, pw as string, proj as string)
CimClearProjectUserPassword(CIMPuser as string, pw as string, proj as string
CimLogin (proj as string)
CimLogout (proj as string)
General Guidelines
The following routines can be called to avoid the CIMPLICITY invoked GUI.
Purpose | To enable an application to have logins reference the set data |
Routines |
GEFCIMPLICITY_setuserpw() or CimSetProjectUserPassword()
|
Description | Use the routine to set the CIMPLICITY user and corresponding password (if there is one) for the project from which resources are about to be requested, Do this before you request any CIMPLICITY resources.
Note: If the provided data is not valid, no attempt is made to obtain the login information via GUI or otherwise, and no error is given. These routines can be called multiple times to change the data that should be referenced on future login attempts without having to clear any data already set.
|
Purpose | To enable an application to stop having logins reference the set data |
Routines |
GEFCIMPLICITY_remuserpw()
or CimClearProjectUserPassword()
|
Description | The routine:
|
Purpose | To force a logout of the currently logged in user |
Routine |
CimLogout
|
Description | After CimLogout is called, either CimLogin must be called or the similar action initiated from the Login Panel, before data can be retrieved again. |
Purpose | To cause CIMPLICITY to initiate a login sequence |
Routine |
CimLogin
|
Description | This most likely will be preceded by a call to CimSetProjectUserPassword and CimLogout , to force a change in the currently logged in CIMPLICITY user. |