Remote Access of CWSERV on Supported Operating Systems
You can access CWSERV from a networked supported operating system using Microsoft NetDDE. This requires that you first set up a DDE Share on the Server node where CWSERV is running. Then, when referencing CWSERV through DDE on the client, you must be sure to indicate that you are using NetDDE. The following are a few notes to help in this operation.
1 | Create a DDE share on the Server node. |
2 | Reference CWSERV from a networked Windows client. |