user_protocol_info

Defines the Device Communications Toolkit features that are supported in this customized communication enabler.

You can find the template for this subroutine in:

usrtm_protin.c

Syntax

void user_protocol_info(int *max_buffer_size,
                        SUPPORT *supported)

Input Parameters

None.

Output Parameters

max_buffer_size

Defines the amount of data (in bytes) that can be transferred between the device and the enabler in one operation.

user_read_data(), user_write_data() and user_process_unsolicited() cannot process more than the max_buffer_size bytes of data.

max_buffer_size may not exceed the size of TOOLKIT_MAX_INTERNAL_BUFFER.

supported

Is a pointer to a structure defining the supported options for the device. SUPPORT is a typedef to a structure defined in <inc_path/toolkit.h> .

Return Value

None.