user_write_data
Writes data to specific memory locations within the device's memory.
You can find the template for this subroutine in:
usrtm_wrda.c
Syntax
void user_write_data(DEVICE_DATA *device_struct,
ADDR_DATA *address_struct,
int length,
char *data,
int *download_req,
int download_comp,
int *comm_status,
int *status)
Input Parameters
device_struct
Is a pointer to the structure defining device data. DEVICE_DATA is a typedef to a structure defined in <inc_path/toolkit.h>.
address_struct
Is a pointer to the address from which the data was read. ADDR_DATA is a typedef to a structure defined in <inc_path/toolkit.h>.
length
Is the number of bytes of data to be written.
data
Is a pointer to the actual data to be written.
For data from bit (TOOLKIT_BIT) domains, bit data is packed into bytes so that the leftmost bit is the most significant.
Bit data is always accessed in multiples of 8 bits, so write requests near the end of a bit domain must ignore extra bits that would be beyond the end of the domain.
For domains whose element size is greater than one byte, the bytes are ordered in the same way as they are ordered by the underlying operating system where the enabler is running.
download_req
Reserved for future use.
download_comp
Reserved for future use.
Output Parameters
comm_status
Indicates whether a status of TOOLKIT_FAILURE occurred as a result of a communication failure. Valid values are:
TOOLKIT_SUCCESS | Failure is not due to communications failure. |
TOOLKIT_WRITE_FAILED | Could not send command or data to device. |
TOOLKIT_TIMEOUT | Sent command or data to device, timed-out waiting for a response. |
TOOLKIT_BAD_DATA | Received response from device but it contained invalid data such as an incorrect checksum. |
TOOLKIT_FAILURE | Failure is due to communications failure. |
status
Indicates whether the function read all the data. Valid values are:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_REPLY_LATER | Write request queued for future processing. |
TOOLKIT_FAILURE | Function did not complete successfully. Check comm_status to see if the failure was the result of a communication failure. |
Return Value
None.