user_write_point_quality
Writes point quality data to the specified device.
You can find the template for this subroutine in:
usrtm_wrtpqual.c
Syntax
void user_write_point_quality(DEVICE_DATA *device_struct,
ADDR_DATA *address_struct,
TOOLKIT_QUALDATA *pqualdata,
int *comm_status,
int *status)
Input Parameters
device_struct
Is a pointer to the structure defining device data. DEVICE_DATA is a typedef to a structure defined in <inc_path/toolkit.h>.
address_struct
Is a pointer to the address from which the data was read. ADDR_DATA is a typedef to a structure defined in <inc_path/toolkit.h>.
pqualdata
Is the pointer to the quality data to be written. TOOLKIT_QUALDATA is a typedef to a structure defined in <inc_path/toolkit.h>.
Output Parameters
comm_status
Indicates whether a status of TOOLKIT_FAILURE occurred as a result of a communication failure. Valid values are:
TOOLKIT_SUCCESS | Failure is not due to communications failure. |
TOOLKIT_WRITE_FAILED | Could not send command or data to device. |
TOOLKIT_TIMEOUT | Sent command or data to device, timed-out waiting for a response. |
TOOLKIT_FAILURE | Failure is due to communications failure. |
status
Indicates whether the function read all the data. Valid values are:
TOOLKIT_SUCCESS | Function completed successfully. |
TOOLKIT_REPLY_LATER | Write request queued for future processing. |
TOOLKIT_FAILURE | Function did not complete successfully. Check comm_status to see if the failure was the result of a communication failure. |
Return Value
None.