DOUT Faceplate: Main Frame
Refer to the following table for descriptions of the fields.

Area | Description |
1 | The description of the current DOUT state. Default descriptions are: Off, On. More descriptive state definitions, which can be entered in the DOUT object’s Properties dialog box, may display instead of On/Off. For example: Open Valve may display instead of Off. Close Valve may display instead of On. |
2 | Forcing is Active when the RAW value is forced. Forcing is Inactive RAW value is not forced. Forcing can be set to Active or Inactive on the Details frame. |
3 | Exit Button. Click to close the faceplate. |