INTERLOCK Faceplate: Details Frame
Refer to the following table for descriptions of the fields.
Area | Description |
1 | Type of device associated with the INTERLOCK block. Can either be 3-state (DC3S) or 2-state (DC2S) device. Question marks display if there is a communication failure on loss of data or invalid data. |
2 | Reports whether or not the device type that is associated with the INTERLOCK block is started. When Yes, the device is started. When No, the device is not started. Question marks display if there is a communication failure on loss of data or invalid data. |
3 | Interlock Polarity Normally Open/Closed. The symbols indicate the interlock’s normal state: Normally Open or Normally Closed. It is configured in the Logic Developer’s Property Inspector. Question marks display if there is a communication failure on loss of data or invalid data. |
4 | Exit button. Click to close the faceplate. |