MANUAL_SP Faceplate: Details Frame

Refer to the following table for descriptions of the fields.

Note: Data entry fields in this Details frame are writable when a user Is associated with both the object's resource and a role that has at least a Level 200. If, after you log in, the data entry fields should be writable and are not, consult your system administrator.
Area Description
1 Manual setpoint minimum value. In order to have scaling, the minimum value must be lower than the maximum value.
2 Manual setpoint maximum value. In order to have scaling, the maximum value must be greater than the minimum value.
3 Exit Button. Click to close the faceplate.