Required Files Location for Process Systems with CIMPLICITY
CIMPLICITY installs the following required Process Systems files in the following Installation folder.
...Program Files\Proficy\Proficy CIMPLICITY\Classes\PPS

Item | Folder/File | Description |
---|---|---|
1 | Faceplate folder | Contains runtime only CimView files that contain Mimic object definitions. |
2 | *.soc files. | Function block class files |
3 | PPS_LIBRARY.cmsrt | PPS runtime-only CimEdit scripts. Note: By default, the GSM_GLOBAL_SCRIPT global parameter will point to the PPS_LIBRARY.cmsrt for the Process Systems installation. |
4 | ppsfaceplates.cache | A cache file that is used with the /loadcache command line option of CimView. PPSfaceplates.cache contains all the faceplates file names and locks them in the cache. It is a plain text file may speed performance when working with the PPS faceplates. However, it is not required. |