Faceplate Translation
About this task
CIMPLICITY's Process Systems faceplate user interfaces can be translated, using the CIMPLICITY Language Mapper and an automatically created translation file Faceplates.clm.
- Faceplate translation.
- Faceplates.clm location.
- Faceplate translation guidelines.
Faceplate Translation
Procedure
- Open the CIMPLICITY Workbench.
- Select Computer>Managed Files in the Workbench left-pane.
-
Double-click classes\pps\faceplates\FACEPLATES.CLM.
Result: The faceplate keys are listed in the file.
-
Translate the keys the same as you would do for any translation in CIMPLICITY.
Faceplates.clm Location
Open the CIMPLICITY installation folder that holds the faceplates files; the path is:
...\Program Files\Proficy\Proficy CIMPLICITY\classes\pps\faceplates
The file, Faceplates.clm, is located in the \faceplates folder.
guide: Faceplate Translation Guidelines- During a CIMPLICITY installation that is an upgrade, CIMPLICITY checks to see if faceplates.clm exists. If it does, CIMPLICITY will not overwrite it; if it does not, CIMPLICITY will create it.
- A file Faceplates_src.clm is also located in the faceplates folder. Do not use the Faceplates_src.clm file. Faceplates_src.clm will be overwritten when CIMPLICITY is re-installed or upgraded.
When CIMPLICITY is upgraded, Faceplates_src.clm may have some new translation keys. These keys will have to be merged into an existing Faceplates.clm in order to make them available for translation.
- If you want to create a new Faceplates.clm, copy and paste Faceplates_src.clm into the \faceplates folder and rename the copy Faceplates.clm.