Dynamic Mode Imports
Dynamic mode import lets you import point information without shutting down and restarting a project. To perform an import in dynamic mode you must use the command line option –y as described in the following example:
clie import myfile.csv -y
The CIMPLICITY Login dialog box will ask you to log into the project if you have not done so.
If you attempt a dynamic import while the project is not running, the import will continue in static mode and display the following warning message:
Project must be running to use dynamic configuration.