Enumeration Point Application Examples
- A point is assigned an enumeration set.
- Enumeration applications include the Point Control Panel and CimEdit/CimView.
A Point is assigned an enumeration set
- A UDINT analog point named HEAT.SOUTH.REGION.01_MACHINE6501:
- Allows setpoints.

- Is associated with an Enumeration set named TEMPERATURE.

- The TEMPERATURE values/text are as follows.

Value | Text | Setpoint Allowed |
---|---|---|
0 | Too Cold | True |
1 | Cold | True |
2 | Normal | True |
3 | Warm | True |
4 | Hot | True |
5 | Too hot | True |
Enumeration applications include the Point Control Panel and CimEdit/CimView.
The Enumeration set is used in:
- The Point Control Panel.
- CimEdit/CimView.