Point Procedures in the Point Control Panel
There are some procedures that you can perform in the Point Control Panel that apply to any points, including points in manual mode and points with alarms.
You can:
1 | Add points to the Point Control Panel. |
2 | Change Font Colors in the Point Control Panel. |
3 | Edit a Point through the Point Control Panel. |
4 | Delete a Point from the Point Control Panel. |
Note: An Invalid Point icon
will appear to the left of the Point ID if the point is not valid. This can happen, for example, if you add a point to a Point Control Panel file, save the file, close it, then delete the point from the project when you are working in the Workbench. The next time you open the Point Control Panel file an Invalid Point icon will appear next to that Point ID.