Additional Roles {<filename>.rol} file Imported

Procedure

  1. Create a second file called <filename>.rol where <filename> is the same as the CSV file.
  2. Add one line in <filename>.rol for each point that you are routing to roles other than SYSMGR, USER, or OPER. The format of the line will be the Point ID followed by a list of roles. Separate each field with a comma.
  3. Run the Import utility as usual. The utility will automatically search for a .rol file whose name matches that of the CSV file, and process the additional role information.

    The following is an example of an .ROL file:

    ##  Point Role File Ver. 1.1
    ##  File created by:  GE Intelligent Platforms, Inc. -- CIMPLICITY  Ver.  8.1
    ##  File created at:  15:33:35  on 6/21/95
    ##
    TEST_ANALOG,DOER,FIXER
    TEST_DIGITAL,FIXER