Configuration Data Deleted
About this task
You can use the CLIE utility to delete point information from the CIMPLICITY database.
todo:
To delete CIMPLICITY point data:
Procedure
- Start a command shell in the project from which you want to export data.
-
At the system prompt, invoke the following command:
$ clie delete < point_id> [/NOCONFIRM]
Where
< point_id> is the Point ID you want to delete. You can use the wildcard characters ? and * to delete sets of Point IDs.
The optional argument for the delete command is:
Argument Decription /NOCONFIRM Deletes the requested points without prompting you to confirm the deletion. If you choose to confirm the deletion, you are prompted like this:
> clie delete D?I* Starting Import/Export - logging to LOG_PATH:IC169.log Do you want to DELETE <DRIVE_CONVEY1> (Y)es (N)o (A)ll y Do you want to DELETE <DRIVE_CONVEY2> n Number of points Deleted = 1 Successful completion - Review LOG_PATH:IC169.log log file for messages. >