Display Selected Fields in the Workbench
About this task
- Select fields to display in the Workbench.
- Field selection.
Select Fields to Display in the Workbench
Note: Two useful fields that display the point status are:
Needs Update… | Displays a one (1) if a point configuration has changed and the project needs a configuration update. |
Modified | Displays the date when the point was last modified |
Field Selection
About this task
Procedure
- Select Points in the left pane.
-
Use any of the following methods to open the Field Chooser dialog box.
Method 1
- Click the right mouse button in the right pane.
- Select Field Chooser… from the popup menu.
Method 2
- Click View on the Workbench menu bar.
- Select Field Chooser.
Method 3
Click Field Chooseron the Workbench toolbar.
The Field Chooser dialog box for points opens when you use any of these methods.
A Fields that will not display. B Fields that will display. C Add/Remove Fields to and from the display list. D Moves a selected field further left in the pane. E Moves a selected field further right in the pane. F Accept/cancel changes in the display list.