Open an Existing Attribute Set Dialog Box
About this task
CIMPLICITY provides several methods to open an Attribute Set dialog box for an existing attribute set.
- Workbench
- Point Properties dialog box's Advanced General tab
Workbench
Procedure
- Select Project>Points>Attribute Sets in the Workbench left pane.
- Select an attribute set in the Workbench right pane.
-
Do one of the following.
A Click Edit>Properties on the Workbench menu bar. B Click the Properties button on the Workbench toolbar. C In the Workbench left pane: - Right-click Attribute Sets.
- Select Properties on the Popup menu.
D In the Workbench right pane: Either Or Double click an attribute set. - Right-click an attribute set.
- Select Properties on the Popup menu.
E Press Alt+Enter on the keyboard. Result: The Attribute Set dialog box opens with the selected attribute set.
Point Properties dialog box's Advanced General tab
- Right-click Attribute Sets.
- Select Properties on the Popup menu.
- Right-click an attribute set.
- Select Properties on the Popup menu.
- Select the General tab in the Point Properties dialog box for the point you are configuring..
- Click Advanced to put the General tab in advanced mode.
- Select the point attribute set in the Attribute set field that will be modified.
-
Click the Popup Menu button; select Edit on the Popup menu.
Results
The Attribute Set dialog box opens with the selected attribute set.