Estimate the Number of Screens for a Project
When you have determined your information requirements, you can estimate the number of screens that need to be designed. The number will be influenced by the:
- Anticipated number of viewer destinations that require different screens
- Type and number of monitoring and regulating tasks that can be divided into logical units
- Amount of information to be displayed, keeping in mind that displays need to be clear to view in a runtime environment
Using frames is another layout option if you have several objects on a screen that will change during runtime, based on a similar set of conditions.