Typical Windows Application Tasks Available in CimView
The following typical Windows application tasks are available in CimView.
1 | Open other CimView screens through an open CimView screen. |
2 | Flush cached screens. |
3 | Distribute copies of the screen or screen file. |
4 | Select whether or not to display the toolbar, menu and/or status bar. |
5 | Go back to the previous screen or an Overview (home) screen, if there is one. |
6 | Change the size of (zoom) the CimView screen and window that you are viewing. |
Note: The features and behavior described are the default settings. You system may vary due to customized configuration.