Enter a Value for a Setpoint
About this task
A value setpoint enables you to enter a value for a point on the CimView screen.
- Setpoint: Enter Value.
- Setpoint: Cancel Value Entry.
- Example: Setpoint in CimView.
Setpoint: Enter Value
Procedure
- Select the object.
-
Do one of the following to activate the object for editing:
- Press Enter on the keyboard or
- Click the object with the left mouse button.
-
Enter the new value for the setpoint.
You can use Ctrl+Z to undo a single level of editing.
-
Press Enter or Tab to perform the setpoint.
Note: If you press Tab, the next action object is automatically highlighted.
Results
The new value for the point displays in the Setpoint object.
Setpoint: Cancel Value Entry
Do one of the following.
- Move the cursor away from the object; click the left mouse button.
- Press Esc on the keyboard.
Example: Setpoint in Cinview

1 | Current point value |
2 | Setpoint being changed. |
3 | New point value displays |