Open the Point Control Panel through CimView
About this task
Note: Viewing the Point Control Panel through CimView is available if the role assigned to your user ID has authorization .
The Point Control Panel provides you with a forum in which you can easily review and change point values and status during runtime.
Procedure
- Right-click the CimView screen or an object.
-
Select Point Control Panel on the Popup menu.
Results
The Point Control Panel opens displaying the points that are configured for the CimView screen or the selected object.

Note: If there are no points associated with the selected object, a message informs you. The Point Control Panel does not open.