ExtDec_api_send_decision
The ExtDec_api_send_decision function sends a decision buffer to the RCO. If the external process is unable to return a decision, this function should be called after setting the dec_quantity field to zero in the PDC_CTRL_DECISIONS structure.
Syntax:
COR_14 ExtDec_api_send_decision
(DADDR*addr,PDC_CTRL_DECISIONS*ctrl_loc_dec,COR_STATUS*)
Input | |
addr | Address of RCO process that will receive decisions. |
Ctrl_loc_dec | Pointer to structure containing a list of control decisions. |
Output | |
Restat | Pointer to status structure. |
Return Value:
Either COR_SUCCESS, COR_WARNING or COR_FAILURE. If the function returns COR_WARNING or COR_FAILURE, additional error information can be found in restat.err_msg and restat.err_code.