Non-Serialized Items: Defined
Non-Serialized items are parts, assemblies or other articles that you are not interested in positively identifying, but you want to know their location.
Non-Serialized items:
- Do not have a unique identifier.
- Hold two attributes, a parent ID and an item type.
- Do not require a tag for sensor recognition.
- Can be pallets, carriers, bins or other articles that are reused in production.
Example
The following diagram shows a cart, which is an item that is reused in a factory,and trips a limit switch that is at the entry point of a Carriage Return Region 5 (CR5). The tracking system is notified that an item has passed into CR5.

1 | CIMPLICITY server with the Tracking system. |
2 | Simple limit switch signal the tracking system that something passed. |
3 | The server receives the signal. |