PRT Client Startup: prtclnt_route.cfg
The layout of prtclnt_route.cfg that is shown here is the same as in the existing configuration files.
|-* IDT file generated by IDTPOP utility v1.0
* RECORD: PRT_ROUTE Production Tracking Route
*
* 0 orig_region_id ID of region item exits
* 1 dest_region_id ID of region item enters
* 2 item_type_id ID of type traveling between regions
* 3 transition_ptid ID of transition point between regions
* 4 set_ptid ID of point to be set on transition
* 5 translation_id ID to interp type trans indicator
* 6 transition_type_code transition indicator type code (1-8)
* 7 process_first_ptchange Should we process the first point change
*
*A_TP1|\\PA3\LONGREGIONNAME_T||A1_A3_ITEMID|||3|1
*A_TP1|\\PA3\LONGREGIONNAME_T||A1_A3_ITEMID|||4|1
*A_TP1|\\PA3\LONGREGIONNAME_T||A1_A3_ITEMID|||1|1
*A_TP1|\\PA3\LONGREGIONNAME_T||A1_A3_ITEMID|||7|1
A_TP1|\\PA3\LONGREGIONNAME_T||A1_A3_ITEMID|||8|1
A_TP1|\\PA3\B_TP3||A1_X_B3|||5|1
B_TP1|\\PA2\A_TP2||B1_A2_ITEMID|||3|1
B_TP1|\\PA3\A_TP3||B1_X_A3||XLATE1|6|1