PRT_ITEM_TYP

The PRT Item Type (prt_item_typ) configuration file is used to define all of the item types that the Tracking Model is responsible for monitoring.

OPTIONAL FILE

The fields are:

No. Field Name Description Data Type Entry Example
0 item_type_id Unique name for the item type. 16 characters COMPRESS
1 item_type_code Unique code identifying the item type to be sued internally by PRT. Integer 4
2 item_type_desc Textual description of the item type. 40 characters Compressor Item Type
3 item_tracking_type Code identifying the tracking type: One byte 1
1 Serialized
2 Non-serialized
4 item_class_id Name of the item class to which this item type belongs. Note: Item Classes are not required but are recommended. One item class can be created for all item types. 16 characters Refrig