Broadcast Queue Manager Job File Locations

Procedure

  1. Right-click CimForms in the TrackerCfg_UI.
  2. Select Properties on the Popup menu.

    A CimForms Properties dialog box opens.

  3. Change any default paths, if needed.

    Paths are as follows.

    Field Description
    Text Editor Path Location of the text editor that you want to use to create and edit Control Character Token files and ASCII forms.
    Opens a Select the Text Editor browser.
    Default ...Program Files\Proficy\Proficy CIMPLICITY\exe\CimFormsEditor.exe.
    Spool Location Location for active and history job files. Broadcast organizes folders and jobs as follows.
    1. A project folder is created in the specified location.
    2. Active and History folders are created in the project folder.
    3. Printer folders are created in both the Active and History folder.
    4. Active and History job files are moved to the appropriate folder.
    Opens a Browse for Folder browser.
    Default C:\Temp\IBC1
    Location for archived files. Broadcast organizes the folders and jobs as follows.
    1. A project folder is created in the specified location.
    2. An Archive folder is created in the project folder.
    3. Printer folders are created in the Archive folder.
    4. Archived job files are moved to the appropriate folder.
    Opens a Browse for Folder browser.
    Default C:\Temp\Archive