Simulated vs Playback mode
|
Simulated execution mode |
Playback execution mode |
|||
Source block type |
Historical |
Real-time |
Historical |
Real-time |
Real-time |
Source block configured mode |
Historical |
Not available |
Historical |
Historical |
Real-time |
External data used for blueprint execution |
Historical data |
Not available |
Historical data |
Historical data |
Real-time data |
Rate of execution |
As quickly as possible. As soon as the blueprint has executed on one data record, it starts with the next. |
Not available |
Determined by sampling rate in the data. The blueprint executes at the recorded data timestamps. Thus, if the historical data records are 10 minutes apart, the blueprint will only execute every 10 minutes, and continue until it has executed on the entire dataset. |
Determined by sampling rate in the data. The blueprint executes at the recorded data timestamps. Thus, if the historical data records are 10 minutes apart, the blueprint will only execute every 10 minutes, and continue until it has executed on the entire dataset. |
Determined by the sampling period configured in source block. |
Limits on blueprint execution |
No limits. Simulated mode enables visualization at a faster rate than playback mode. |
Not available |
There is a 2-day limit on running blueprints in playback mode. |
There is a 2-day limit on running blueprints in playback mode. |
There is a 2-day limit on running blueprints in playback mode. |
Graphic display of executing blueprint |
Yes, using configured probes and the Trendviewer. |
Not available |
Yes, using configured probes and the Trendviewer. |
Yes, using configured probes and the Trendviewer. |
Yes, using configured probes and the Trendviewer. |