Configuring the Field Statistics block
The Field Statistics block editor page enables the user to adjust the quality threshold. The quality threshold may be configured as a real value between 0.0% and 100.0% or be adjusted in real time based on a parameter field supplied on the parameter port.
Quality Threshold
The value of the Quality Threshold determines the percentage of the fields in the input port required to be of good quality for the output fields in the statistics port to be marked as of quality good.
The quality of the output fields in the quality port is always good.
Example :
INPUT FIELDS
OUTPUT FIELDS
Related topics: