Configuring the Inactivity Detector block

  1. To open the Inactivity detector block property page (the page on which the block configuration is specified), either double click on the block or right-click on the block and select Block Properties.  

  2. The block automatically creates a set of output fields with the same names as the input fields, the default inactivity period is 0 seconds. The inactivity period must be specified in seconds.

  3. To change the inactivity period for a particular field, single click twice on the value to be changed in the Inactivity Period (seconds) list (in the Fields window) then type the new value in its place.

  4. To specify the same inactivity period for all the fields, type the inactivity period in the Inactivity Period in seconds box and click on Apply to all.

  5. The quality column can be changed to select whether the quality of an inactive field should be marked as bad or left unchanged. Single click to select the item and double click the new selection to update the change.

  6. To specify the same quality for all the fields, select the item in the Change Quality box and click on Apply to all.


Related topics:

  

CSense 2023- Last updated: June 24,2025