Configuring the OPC Classic Server Sink block

Configuring the OPC Classic Server Sink is as easy as specifying the group name and selecting the input fields that must be made available as OPC Classic items.

Return to Overview of OPC Classic Server Sink block

Configuring the OPC Classic Server Sink block

  • The group name is entered in the OPC Group name edit box. The block will not allow the blueprint to run if the name is empty.

  • All the fields in the input port are listed in the Available Fields list.

  • The fields that will appear as OPC Classic items are listed in the Selected Fields list.

  • To move a field from the Available Fields list to the Selected Fields list, select the field and click on . A double-click on the field in the Available Fields list will also move the field over.

  • To move a field from the Selected Fields list to the Available Fields list, select the field and click on . A double-click on the field in the Selected Fields list will also move the field over.

  • To move all the fields to the Available Fields list click on .

  • To move all the fields to the Selected Fields list click on .

Return to top


Related topics:

  

CSense 2023- Last updated: June 24,2025