Field Selector block
The Field Selector block allows the user to decide which fields should continue to be used by the blueprint.
Field Selector block
Description
The Field Selector is used to select a subset of the fields in the input port as fields in the output port of the block. For every input field that is selected there is a corresponding, identical, output field. In order for the blueprint to be runnable, at least one field must be selected.
Field Selector block
Block Type
General
Input/Output ports
The input fields enter through the block input port
The selected fields are placed in the block output port
Functions performed on tags
The Field selector block does not alter the value, timestamp or quality of a field in any way.
Related topics: