Port Combiner block
Combine the fields of 2 or more ports into 1 port.
Port Combiner block
Description
Combines all the files of 2 or more input ports into 1 port. If 2 or more fields have identical names the port number is appended to distinguish the fields. Thus the output port will have all the fields of all the input ports.
Port Combiner block
Block Type
General
Input/Output ports
The number of input ports are set in the configuration, and must be ≥ 2 and ≤ 100 by default. Every input port may have any number of fields of any type.
Functions performed on tags
The output values, time stamps and qualities are copied from the input fields.
Related topics: