Troubleshooting the PCA Model block
Return to:
Configuring the PCA Model block
Design Time Runnability
ERROR REPORTED |
ACTION REQUIRED |
No PCA model loaded. |
|
No window size was specified when using the Moving Window calculation method. |
Configure the calculation method: Moving Window: specify the window size in seconds. |
No trigger field was selected. |
Configure the calculation method: Batch:Select a trigger field. |
The selected trigger field cannot be found in the parameter port when using the Batch calculation method. |
Input port & Parameter port: Link the text data source to the parameter port. |
All of the model input fields are not mapped to the data source input fields from the Input port. |
Run-Time
If the user is using Moving Window or Batch calculation methods, then the block could give an error if:
ERROR REPORTED |
ACTION REQUIRED |
WILL IT STOP THE BLUEPRINT? |
One of the input fields gives a different value or quality for the same timestamp in two consecutive executes. |
Check your solution blueprint for any changes made to the timestamp. If data values are changed at all, the timestamp must be changed, and the timestamp must have increased from the previous one. |
Yes |
The timestamp of one of the input fields for an execute is older than the timestamp for that field on the previous execute. |
Check your solution blueprint for any changes made to the timestamp. If data values are changed at all, the timestamp must be changed, and the timestamp must have increased from the previous one. |
Yes |