Troubleshooting the Nonlinear Classification Model block
Return to:
Nonlinear Classification Model block
Configuring the Nonlinear Classification Model block
Design Time Runnability
ERROR REPORTED |
ACTION REQUIRED |
The model is not trained. |
During model construction and configuration, it must be trained by the using the Offline Trainer block. |
The input port does not contain all the fields used during configuration. |
All the fields required by the model cannot be found in the input port. The fields that are missing will be listed. |
The model was trained on more inputs than are provided in the input port. |
There are too few input fields in the input port. The input port must only have the fields required by the trained model. This happens when the model was constructed on say 5 fields but only 4 or less were given in the input port. The fields that do not belong in the input port will be listed. |
The input port contain fields that are a different type than the fields that were used during configuration. |
One or more of the field types in the input port differ from the types required by the model. The fields with the incorrect types will be listed. |