Known Issues
Defect # |
Area |
Description |
DE13340 |
Blocks |
The Lookup Table 2D block output field values may change without updating timestamps. |
DE19811 |
Architect |
Architect may stop and exit unexpectedly when converting a field to double in the Text Source block property page. |
DE69230 |
Blocks |
When OPC Client Source and Sink blocks reconnect to a CSense OPC Server, both client and server Action Objects may go into an error state. |
DE131928 |
Architect |
Executing a block in the Architect that was previously published to the Analytic Repository with statefull execution enabled, may cause the Architect to terminate unexpectedly under certain conditions. |
DE135748 |
Blocks |
Under specific conditions, the Historian Source Block may produce incorrect Field timestamps when the block is configured to execute in real-time mode. |
DE136488 |
Blocks |
The Optimized DB Sink block fails to reconnect to SQL Server on connection failures. |
DE136862 |
Blocks |
The template block 'Full Runnability Check' and 'Expansion' fails if the template contains an output port block that was configured to be locked, but not all the output fields were used. |
DE137735 |
Architect |
Architect hangs when connecting to Oracle with a non SYSDBA user using the Tabular blocks. |
DE137907 |
Blocks |
The Optimized DB Source block is unable to retrieve data from Oracle. |
DE137915 |
Continuous Troubleshooter and Discrete & Batch Troubleshooter |
Under specific conditions when opening a previously saved Troubleshooter project, open Data Preparation views may continue to display a ""Loading"" message without recovering. |
DE137920 |
Continuous Troubleshooter and Discrete & Batch Troubleshooter |
The Database Table import operation displays an error message when the user does not have access to the first table in the list. |
DE137921 |
Continuous Troubleshooter and Discrete & Batch Troubleshooter |
Oracle Oledb driver fails when used with the Database Table Import operation. |
DE138344 |
Continuous Troubleshooter and Discrete & Batch Troubleshooter |
The Replace Partial Strings data recipe operation may not replace strings that contain special characters consistently. |
DE140469 |
Blocks |
For specific conditions, blueprints with Historian source blocks configured via the SDK may return different field timestamps on first execute when compared to blueprints with Historian source block configured using the Architect. |
DE148898 |
Blocks |
When a blueprint contains a feedback loop before model inputs, the offline trainer fails to train the model and reports and error. |
DE149486 |
MPC Editor |
When removing MVs from the configuration in the MPC Editor, the Model section information is lost. |
DE149622 |
Licensing |
CSense may report license expiration if 1 of multiple licenses has expired in the License Client. |
DE153369 |
Discrete & Batch Troubleshooter |
Under specific conditions, X-axis labels on the Pivot Tables in the Discrete and Batch Troubleshooter may overlap and become illegible. |
DE154488 |
Blocks |
Text Sink roll-over produces too many files when reading data sampled at 1 second intervals. |
DE155300 |
Blocks |
Changing the Date Time format of the machine to English on a Japanese OS may cause some property lists to show corrupted text. |
DE155985 |
Blocks |
The PLS Analysis block may generate too many score fields for certain models. |
DE155986 |
Blocks |
The PLS Analysis block does not produce VC values for some input fields when running over a moving window. |
DE156065 |
Blocks |
The PCA Block returns inconsistent timestamps on output fields when using a trigger field. |
DE156861 |
Continuous Troubleshooter |
Scenario Analysis sliders cannot be moved in Continuous Troubleshooter. |
DE157723 |
Blocks |
The Feedback block property page filters may cause exceptions to be shown when filtering the list of feedback fields for Timestamps or Initial Quality. |
DE158346 |
Blocks |
OPC Client I/O Blocks incorrectly display the supported version for OPC HDA connections as 1.0. The value should read 1.1. |
DE159585 |
Data Preparation |
The Data Preparation Merge operations fail when importing fields with matching names and differing cases. |
DE159754 |
Continuous Troubleshooter |
The ""Export"" button on the SPC+ main view in the Continuous Troubleshooter exports incorrect values for all cells in the exported CSV file. |
DE161011 |
Continuous Troubleshooter |
For specific data, the histogram in the Continuous Troubleshooter may display illegible and overlapping text on the x-axis. |
DE161013 |
Continuous Troubleshooter |
Under specific conditions the Reconfigure operation may be incorrectly enabled for some datasets when a dataset is loaded in Step 2 of the Continuous Troubleshooter. |
DE161122 |
Continuous Troubleshooter |
The Knowledge Extraction view in the Continuous Troubleshooter may display truncated text on in the playback controls on certain screens. |
DE161998 |
Blocks |
OPC UA Sink executes even if no connection was configured. |
DE162590 |
Discrete & Batch Troubleshooter |
The Discrete and Batch Troubleshooter may display empty data when plotting string vs string scatter plots. |
DE162902 |
Continuous Troubleshooter and Discrete & Batch Troubleshooter |
Cannot load a dataset in one Troubleshooter while importing data on another instance of the Troubleshooter on the same machine. |
DE164313 |
Architect |
Overloads are shown when executing a blueprint in the Architect in Playback mode when the sampling period is set to Raw by time for a Historian source block. |
DE164315 |
Architect |
Under specific conditions when executing a blueprint in Playback mode in the Architect, a user may be unable to Stop execution. |
DE164565 |
Blocks |
Under certain conditions, the MPC block execution may produce a division error when using slope control. |
DE164889 |
Data Recipes |
When transposing field names that has special characters using the Transpose operation in a data recipe, the names are not auto corrected(not replaced with underscore). |
DE165552 |
CSense Runtime Manager |
After completing an upgrade from a previous version of CSense, real-time Action Objects that were running prior to starting the upgrade may not automatically start up after installation. Restarting the CSense Runtime Service or the machine will restart all previously deployed Action Objects. |
DE167874 |
Data Recipes |
In the Continuous Troubleshooter, the Text file import operation may not detect all Fields correctly under specific conditions. |
DE168111 |
CSense Runtime Manager |
During blueprint deployment, some failures and related exceptions may not be logged, resulting in a silent failure. |
DE170549 |
Blocks |
There is a mismatch between the description of output fields for the MPC Block in the help documentation and the actual outputs produced by the block. |
DE171768 |
CSense |
Some displayed text on CSense screens may not be translated to your language. |
DE171769 |
Blocks |
The Close button on Min Max block & Timestamp filter doesn't close the property page. |
DE172450 |
Continuous Troubleshooter |
Continuous Troubleshooter projects that contain system identification items cannot be used between different supported languages. |
DE176485 |
Continuous Troubleshooter |
Numerical columns may not sort correctly in Continuous Troubleshooter. |
DE177243 |
Blocks |
The OPC Client Source block does not work as expected when using async to connect to a CSense OPC Server when deployed in the Action Object Manager. |
DE177960 |
Blocks |
Slow performance while browsing tags using the Historian Source block. |
DE180661 |
Process+ |
Process+ Ad hoc Action Objects do not stop execution after completing execution for the specified data window. |
DE187688 |
Blocks |
Under specific conditions, when running the Historian source block in Historical mode, data will be retrieved in batches of 5000 samples. Expected behavior is for the retrieved batches to contain 2000 samples each. |
DE187820 |
Blocks |
The start and end times for the data window on the Historian Source block is calculated incorrectly when deploying a blueprint as a scheduled Action Object using a Historian source block with the “Use the latest data available” selected for the “Import options” setting, and using “Raw by time” for the “Sampling mode” setting. |
DE189235 |
Blocks |
Source/Sink blocks may generate excessive event log entries when disconnected. |
DE192854 |
Blocks |
The Discovery dialog on the OPC UA Source and Sink Blocks do not display errors. |
DE194567 |
Continous Troubleshooter |
Loop tuning may fail when used in a region that specifies a comma as decimal separator. |
DE195474 |
CSense OPC Server |
Under certain conditions, connections to the CSense OPC Server may fail. |
DE196968 |
Blocks |
OPC UA Client Sink may fail to write tag values to a Honeywell PKS server for specific tag types. |
DE197030 |
Blocks |
The OPC UA Client Source block may produce uninitialized output fields on first execute. |
DE198473 |
Blocks |
While configuring the Tabular Database Source, it is possible to get an invalid value for 'Import options'. |
DE199041 |
Architect |
Playback execution of a blueprint with a Historian Source block in the Architect causes overloads on each execute. |
DE199291 |
Data Recipes |
For the Import Control Loop Data operation in data recipes, a user can click Finish when no loops are selected. |
DE199294 |
Data Recipes |
Invalid configuration can be executed when going to a previous page with valid configuration in the Import Control Loop Data operation in Data Recipes. |
DE199375 |
CSense Runtime Manager |
Removing a large number of real-time action objects in the CSense Runtime Manager may cause entries to be left behind in the grid. |
DE199377 |
CSense Runtime Manager |
Removing a large number of scheduled Action Objects in the CSense Runtime Manager may cause the Runtime Manager to become unresponsive until all the Action Objects are removed. |
DE199379 |
CSense Runtime Manager |
Deploying a large number of invalid event based action objects in the CSense Runtime Manager may require the user to click through multiple dialogs to clear the displayed error messages. |
DE199443 |
Data Recipes |
The Finish button is not consistently enabled for a valid configuration in the Limit Values operation in Data Recipes. |
DE199488 |
CSense Runtime Manager |
Triggering an event based action object using the CSense SDK on the same execute time causes the execution to fail. |
DE199535 |
CSense Installer |
When using the Repair installation option while installing CSense 2023, an error message is displayed indicating that the Services are not able to start. |
DE199705 |
CSense Installer |
CSense 2023 (English) installer is not blocking invalid upgrades from an International version of CSense. Attempting to upgrade from an international version to the English version causes unexpected results. |