Fixed Defects
Defect # |
Area |
Description |
DE166117 |
Continuous Troubleshooter |
Resolved an issue where the timestamps on the System Identification and Control Loop Tuning graphs may display as overlapping labels in the Continuous Troubleshooter. |
DE151948 |
Continuous Troubleshooter and Discrete & Batch Troubleshooter |
Resolved an issue where the incorrect mouse cursor was displayed when resizing the panels on the Knowledge Extraction dashboard for both the Continuous- and Discrete and Batch Troubleshooters. |
DE153270 |
Discrete and Batch Troubleshooter |
Ruler behavior is inconsistent when using the ruler on a leave node of the Decision tree in the Discrete and Batch Troubleshooter. |
DE158341 |
Continuous Troubleshooter |
Exporting a Data file from the Continuous Troubleshooter does not use the system configured date separator for exported timestamps. |
DE154688 |
Python Module Manager |
Removing modules from the Python Module Manager does not always remove the wheel from the backup folder. |
DE153269 |
Discrete and Batch Troubleshooter |
On the Trend view in the Discrete and Batch Troubleshooter, when selecting the Zoom Axes mode from the context menu the selection is not used. |
DE154899 |
Continuous Troubleshooter |
Clicking the Proficy Historian None tag filter results in a NullException on a Japanese OS. |
DE158166 |
Architect |
Attempting to delete a user block from the Architect palette does not remove the block from the palette. |
DE165341 |
Continuous Troubleshooter |
System Identification in the Continuous Troubleshooter may produce incorrect models when performed on input data that contains a change in CV with no measured change in PV or when a step change in CV results in a step change in PV at the same timestamp. |
DE168010 |
Process+ |
Improved consistency in the use of MV in stead of CV on Process+ Reports. |
DE168013 |
CSense Runtime Manager |
Incorrect naming of sections used for Manipulated Variable Distribution on Loop Report. |
DE168015 |
Process+ |
Improved the default sort order for the loop performance table displayed on the Process+ Fleet report. |
DE168037 |
Process+ |
Control modes are now clearly indicated on the Process+ Loop Performance report displays. |
DE168112 |
CSense Runtime Manager |
A SQL connection timeout may be logged by Action Objects when the CPU is saturated at 100%. |
DE168115 |
Process+ |
The deployment time for Action Objects that contain external sources and sinks has been improved. |
DE184272 |
CSense Runtime Manager |
Under specific conditions, users may be unable to Deploy Scheduled Action Objects using the CSense Runtime Manager. |
DE171042 |
Documentation |
Added detailed information about establishing trust, certificate store, and user authentication in the OPC UA Client Source and Sink blocks help topics. |
DE198789 |
Continuous Troubleshooter |
Timestamp labels on the x-axis overlap and make it difficult to read the scaling of the axis labels. |
DE177535 |
Architect |
After expanding templates using the Expand Templates option, Blueprint properties are not copied to the expanded Blueprint. |
DE180314 |
Continuous Troubleshooter |
Simulating different P and I settings fail for Sampling Times other than 1 sec. |
DE180334 |
Installer |
During advanced Installation of the Application Server, the permissions for users are not set up correctly. |
DE181439 |
Security |
Identified a security vulnerability in the version of LibXML used by the OPC UA component in CSense. |
DE182169 |
Continuous Troubleshooter and Discrete Troubleshooter |
Resolved an issue where opening an existing project failed to load in Continuous and Discrete Troubleshooter and displayed "Incorrect syntax near 'Tagname' " error message. |
DE194468 |
Continuous Troubleshooter and Discrete and Batch Troubleshooter |
During reconfiguration in the Continuous and Discrete & Batch Troubleshooter applications, the Limiter operation displays upper and lower values that are different from the configured default values. |
DE183930 |
Documentation |
The description for kurtosis in the Continuous Troubleshooter and Discrete and Batch Troubleshooter help documentation has been updated. |
DE184737 |
Continuous Troubleshooter |
Resolved an issue where Cause+ scenario was not being simulated in Continuous Troubleshooter and a progress dialog was shown at 100% without opening the simulation view. |
DE184779 |
Continuous Troubleshooter |
When you open a deployed Process+ Loop in Continuous Troubleshooter, the descriptions of the loops listed in the Loop Tuning tool do not match the descriptions in the Loop Definition file. |
DE185085 |
CSense Runtime Manager |
Unable to restore Action Objects using a Process+ Backup file when the exported loops already exist in the system. |
DE187148 |
Documentation |
.NET Wrapper Operations missing content for building .NET assemblies. |
DE188091 |
Blocks |
Fixed a defect related to the Machine Learning Model block being unable to load the exported data from different regional settings. |
DE189325 |
Blocks |
Resolved an issue where the Endpoints from the previous server were not cleared while using Discovery to find available OPC UA servers. |
DE189327 |
Blocks |
Updated the OPC UA I/O blocks to display endpoints of type "server" on the Discovery dial. |
DE190433 |
Blocks |
Resolved an issue where the OPC UA I/O blocks did not connect to OPC UA servers that have an empty certificate. |
DE190434 |
Blocks |
Resolved an issue where the OPC UA I/O Blocks did not recognize the data type of certain items correctly. |
DE190572 |
Security |
The openssl version 1.1.1.n that is used by the Unified Automation SDK has some medium level security vulnerabilities. |
DE191804 |
Python Module Manager |
Because the Python Module Manager backup folder did not exist on the machine after upgrading to CSense 8.5 SP1, clicking the Modules button on the Python Scripting Block in Architect did not open the Python Module Manager. |
DE193865 |
Continuous Troubleshooter |
Continuous Troubleshooter closes unexpectedly when editing a SysID model after cancelling the option to unload a dataset. |
DE194285 |
Installer |
Installation fails while creating the csense_db_user login with a password longer than 12 characters due to password policy violation. |
DE153272 |
Architect |
Resolved an issue where setting a custom scale on a Probe Group in the Architect displayed a message indicating that the configured value is not a valid number. |
DE172360 |
Discrete and Batch Troubleshooter |
When exporting data from the CSense Troubleshooter, the decimal separator is always a comma, regardless of the regional settings specified for the target machine. |
DE194582 |
Process+ |
Numeric columns on Process+ report grids do not show numeric searching options. |
DE196809 |
Architect |
When the OPC UA Server reports a failure for the write operation of a tag, the OPC UA Client Sink Block will log a single write error for that tag and stop the write operation until the connection is reset or the Blueprint is restarted. Based on the type of error, the Block will trigger the disconnect or reconnect action. |
DE199050 |
Architect |
The Event-based Action Object executes with a different window size than what was configured during the DeployedEventBasedActionObject.ExecuteWindow call. |
NA |
Documentation |
Resolved several minor documentation-related issues. |