Known Issues
Defect # |
Description |
86971 |
Process+ Loop Information dialog resizing is not working as expected in the Runtime Manager. |
87127 |
Data Link Dialog does not allow editing existing connections. |
87646 |
Inactivity Detector block incorrectly lists Array Fields in the property page. |
141780 |
I/O Sink blocks do not verify imported fields against fields in the input port. |
145722 |
Pressing F1 on an operation in Continuous Troubleshooter does not open context sensitive help. |
146793 |
When using the Import Loop Data operation in Data Preparation, a user may select Finish when no loops are selected. |
146797 |
When using the Import Control Loop Data operation in Data Preparation, an invalid configuration can be executed when going to a previous page with valid configuration. |
147362 |
Removing a large number of real-time action objects in the CSense Runtime Manager causes entries to be left behind in the grid. |
147386 |
Removing a large number of scheduled action object in the CSense Runtime Manager, causes the application to become unresponsive until all the work is done. |
147388 |
Deploying a large number of invalid event-based action objects in the CSense Runtime Manager causes the user to click a lot of dialogs to get back to the manager. |
147467 |
For some configurations, the finish button is not enabled with a valid configuration for the Limit Values operation in Data Preparation. |
147647 |
Triggering an event-based action object on the same execute time twice causes the second execution to fail. |
147696 |
Deploying a Process+ action object that does not use all the CONTROL_MODE values generates a warning in the event log indicating compiler warnings. |
147700 |
Cursor is not set to busy while refreshing after Adding or removing modules. |
148170 |
Loading and saving a copy of a blueprint using the SDK fails for NN Classification and Non-Linear Model for Russian translations. |
148793 |
Real time Data Sources Blocks may return data with timestamps that are after the execute timestamp. |
149452 |
Using the SDK to import/export Non-Linear Model does not work on French and Russian operating systems. |
150088 |
Installer may indicate success even though services failed to install. |
150090 |
Event IDs are incorrectly logged as 0 for CSense services event log entries. |
150151 |
Control Loop Import Operation execute fails on French and Russian operating systems. |
150244 |
The Model Alarming block configuration page may display garbled headings for list views contained on the page. |
150309 |
Histogram configuration dialog in data preparation cannot resize to show the full field names for long names. |
150354 |
Architect becomes unresponsive when executing a blueprint with analysis views a second time when the Setpoint, Lower Limit or Upper limits are mapped to fields. |
151281 |
Users may be able to export a blueprint containing source and sink blocks as an ISV Object. |
151562 |
In the Discrete and Batch Troubleshooter, the Data Preparation ribbon is not displayed in some cases. |
151567 |
The Data Summary Statistics view in the Discrete and Batch Troubleshooter may resize and layout controls incorrectly under specific conditions. |
151791 |
The table of contents and search features in the SDK Objects and Methods Offline help are not working as expected. |
152893 |
Grid Lines option on the PCA Simulation View in the Discrete and Batch Troubleshooter is not working as expected. |
152898 |
Architect probe view x-axis and ruler not displaying micro-second resolutions. |
174177 |
OPC Client Source does not work as expected when using asynchronous to connect to a CSense OPC Server and when it is deployed in the Runtime Manager. |
175030 |
Browsing tags using the Historian Source block in the Architect or using the Process+ Action Object Deployment dialogs may take unexpectedly long. |
175867 |
Process+ Ad hoc Action Objects do not stop after executing over the specified window. |
209699 |
Under specific conditions, X-axis labels on the Pivot Tables in the Discrete and Batch Troubleshooter may overlap and become illegible. |
210532 |
Changing the Date Time format of the machine to English on a Japanese OS may cause some property pages to display corrupted text. |
210825 |
PLS Analysis block may incorrectly generate additional score fields for certain models. |
210834 |
The PLS Analysis block does not produce VC values for some input fields when executing over a moving window. |
210878 |
The PCA Block may return inconsistent timestamps on output fields when using a trigger field. |
210989 |
The CSense installer may fail to delete all primer files on exit. |
211235 |
Under certain conditions, the scenario analysis sliders on the Knowledge Extraction view cannot be moved in Continuous Troubleshooter. |
211618 |
Using the filters on the list view in the Feedback block property page may cause exceptions. |
211656 |
OPC Client I/O Blocks display incorrect supported versions for OPC HDA connections. |
211977 |
The merge operations in data preparation may fail with an exception when importing fields with matching names with differing cases. |
212130 |
Using the SPC+ View Export button in the Continuous Troubleshooter may export a CSV file with bad data. |
212826 |
The Histogram in the Continuous Troubleshooter may display garbled text on the x-axis for some data ranges. |
213790 |
The OPC UA Sink block allows execution even when no connection was configured. |
214443 |
The Discrete and Batch Troubleshooter may display empty data when plotting string vs string scatter plots. |
215662 |
Users may be unable to load a dataset in one Troubleshooter while importing data on another Troubleshooter. |
215781 |
Failing to remove a database during uninstall may cause all remaining databases not to be removed. |
215907 |
Python module backups may remain behind in the CSense Program files directory when uninstalling CSense. |
216733 |
When using data preparation in the Discrete troubleshooter to transpose field names that has special characters, the names are not auto corrected, leading to unexpected behavior. |
217004 |
Uninstalling CSense may leave certain files behind on the target system. |
217753 |
The Text file import operation in data preparation may always consistently detect all fields in imported files. |
218178 |
Some screens may not show as translated for operating systems other than English. |
218461 |
Continuous Troubleshooter projects that contain system identification items cannot be used between different supported languages. |
239723 |
Installing CSense 2024 on a French OS may display some of the error dialogs in English. |
240314 |
Using .bit0 and .byte0 in the CSense scripting block causes the block to fail during execution. |
264218 |
The Lookup Table 2D block may produce field value changes without updating timestamps under specific conditions. |
264256 |
Architect may close unexpectedly when converting a field to double in Text Source. |
264489 |
Reconnection behavior for the OPC Client Source and Sink blocks to a CSense OPC Server while deployed as an Action Object may cause both Action Objects to go into an error state. |
265011 |
Under specific conditions, the Historian Source Block may produce incorrect Field timestamps when the block is configured to execute in real-time mode. |
265085 |
Blueprints containing an Optimized DB Sink does not reconnect to SQL Server when connection is lost when deployed as an Action Object. |
265144 |
Template block runnability and expansion may fail if output port blocks are not configured correctly. |
265218 |
Architect may become unresponsive when connecting to Oracle with a non SYSDBA user. |
265233 |
Unable to retrieve data from Oracle using the Optimized Database source block. |
265243 |
Data Preparation views can get into a state of showing 'Loading' and never recovering under certain conditions. |
265265 |
The Database Table import operation displays an error message when the user does not have access to the first table in the list of available tables. |
265269 |
The Oracle OLE DB driver fails with Database Table Import operation. |
265396 |
Replace Partial Strings operation in data preparation is not replacing special characters as expected. |
265420 |
The timestamps of the First Execute may be inconsistent between blueprints configured from the Architect and the SDK under certain conditions. |
265427 |
The CSense SDK Help contains errors regarding missing parameters and return types. |
265703 |
The offline trainer may fail to train a model if a feedback loop exists in the blueprint prior to the model and trainer blocks. |
265871 |
Opening the help documentation for a selected block in the Architect does not open the block help page on a Japanese OS. |
265924 |
The MPC Editor configuration may be lost when removing MVs in certain scenarios. |
265985 |
The License Client always returns expired in CSense if only 1 of multiple Proficy Licenses has expired. |
265988 |
The Summary paragraph on the SDK help documentation for the ActionObjectServer::ActionObjectServer() incorrectly refers to a parameter but the constructor does not take parameters. |
283152 |
The Discrete and Batch Troubleshooter may display additional rulers on the SPE plot that can???t be removed. |
542422 |
Writing to a tag in iFix using the OPC UA Sink block may cause an access violation. |
553101 |
The Variable Contributions plot may disappear in the Discrete and Batch Troubleshooter when using a scroll bar. |
556679 |
Renaming Trend Views in the Trend View Manager in the Continuous Troubleshooter does not work as expected. |
559074 |
Renaming data preparation views through the View Manager dialog is not applied to the open views in the Continuous Troubleshooter. |
559202 |
The Project Explorer in the Continuous Troubleshooter is not updated when the user reconfigures the loaded dataset by adding fields. |
559619 |
Reconfiguring a Rename Field operation on a Random Value dataset in Data Prep result in field names changing incorrectly. |
563386 |
In Data Preparation, the field that displays the string that can be replaced in the Replace String operation is empty when the operation is reconfigured. |
565462 |
Import Control Loop data operation shows SQL Permission error message for non-installing users. |
574504 |
Some outcome classes displayed as part of the rules model in the Continuous Troubleshooter may incorrectly be translated on a Chinese OS. |
574510 |
Exporting the Dataset Summary view in the Continuous Troubleshooter on a Chinese/Japanese OS may export a file with missing entries. |
575833 |
Some block property pages Help button (and F1 hotkey) opens the main Architect help page and not the configuration page for the block. |
577466 |
When using the SDK to configure Source Blocks that support array fields, enabling the Timestamp and Quality fields for arrays does not produce the corresponding fields on the output port of the source block. |
????