Fixed Defects in CSense 2024 SIM 1

The CSense 2024 SIM 1 resolves the issues listed in the table below by updating the respective components.

Case #

(Defect #)

Description

01162484

(622402)
 

The Scheduled Action Object process may not exit when deploying blueprints that contain a Python Scripting block importing some Python modules.

(648507)

In Architect, when the OPC UA Client Source block is connected to an Asix server, users are able to see values for selected fields in the Preview tab but on executing the blueprint, values are returned as zero.

(619182)

Resolved a compatibility issue where some Python modules generated a ‘NoneType’ object has no attribute ‘write’ error when used from the Python Scripting block.

(603876)

The Introduction: Python Scripting topic now includes the list of restricted Python functions/statements in the Python Scripting block.

(588281)

The Python Scripting examples topic now includes updated examples illustrating the use of dictionary methods with Pandas.

(612536)

The Security Best Practices topic now includes important updates on the machine-level DCOM configuration settings.

NA

The SDK Objects and Methods topic now includes links to the SDK help content that was not accessible from the left-navigation pane.

NA

The Event-based Action Objects topic now includes important updates on execution events and execution frequency limits.

Fixed Defects in CSense 2024

Defect #

Description

86880

Unable to create output fields in the Python Scripting block under certain conditions.

87037

The help documentation for the Statistics View in the Continuous Troubleshooter does not indicate that statistic are calculated as time-weighted.

87164

Feedback Block available field list not filtering out mapped fields correctly.

87195

Installation fails when creating the login csense_db_user due to password policy violation.

87196

Not all SQL related errors are logged during installation.

90225

Unable to export Blueprint from Action Deployment in Discrete and Batch Troubleshooter.

141800

OPC UA Client Sink Block fails to write to Honeywell PKS server.

141804

OPC UA Client Source block produces uninitialized output fields on first execute.

142717

Control Loop Performance Monitoring app fails to load when viewing Loop Shift Performance report in Operations Hub.

144225

While configuring the Tabular Database Source Block it is possible to get an invalid value for 'Import options'.

144490

Unexpected Error when browsing an Asix OPC Server address space using the OPC Classic Client Source block.

148913

SPC+ View export in both Troubleshooters may not write the correct data to the output file.

149142

State Cache help documentation does not describe how cache is recovered.

150168

Control Loop Import operation in Data Preparation incorrectly using local time to determine window to query from database instead of UTC.

150246

When using the Import from Source Block operation in Data Preparation and selecting the Historian Source block, the operation may return no values for Raw by Time queries.

150256

In some cases, the Historian Source block operation becomes unresponsive when switching Sampling Mode.

150312

Regional settings are not used when exporting Data from the Discrete and Batch Troubleshooter.

151275

Unable to add a blueprint from the root node to the Template palette.

151776

In some cases, Data Recipes may become corrupted when saved.

151870

The root name of an unsaved blueprint in the Blueprint explorer may display a GUID under certain conditions.

152619

In some cases, the .NET Script Block default script may produce an error for bad quality input.

152907

For specific configuration combinations, the option to Use latest data with Raw by time in the Historian source block may use an incorrect time window.

176940

Execution timestamps may be incorrect when deploying blueprints as Scheduled Action Objects.

177428

The OPC UA I/O Block Discovery dialogs does not display all errors.

208563

Incorrect splitter resize cursor shown on Knowledge Extraction dashboard.

210061

The Text Sink Block roll-over feature may not produce expected result in some cases.

210191

Removing modules from the Python Module Manager does not remove the wheel from the backup folder.

212830

The Reconfigure operation option is not blocked when a dataset is loaded for analysis in the Continuous Troubleshooter.

216410

For some configuration combinations, overloads may be shown during Playback execution in the Architect when using a Historian source block with with Raw by time.

216413

For some configuration combinations, when executing a Blueprint with a Historian source in the Architect using Playback, a user may be prevented from stopping execution due to excessive overload messages.

216559

MPC Controllers may cause a division error when using slope control.

240309

Discrepancy exist between help documentation and available MPC configuration.

265435

Runtime Manager help table of contents is incorrect when help system is launched from the Runtime Manager.

282286

The Tabular Source block can be configured to execute in Real-time mode without a timestamp column causing the results to always output bad values.

282593

Opening the context sensitive help file from the Analytic Repository in the Runtime Manager does not open the help documentation.

290183

The Text Import Operation in Data Preparation may ignore Tabs in text file when a line starts with a TAB.

516244

The documentation for the Clear table on startup feature in the Tabular Sink block requires additional information on required permissions for setup on the database.

519940

Getting Started Guide does not include instructions for setting up SQL Permissions needed to enable csense_db_user when not a SQL Admin.

546757

Incorrect blueprint name is shown in Architect when connecting to a running blueprint.

556533

Exporting a process model from the Continuous Troubleshooter to a folder that the user does not have write access to causes the Troubleshooter to crash.

558992

Exporting Active Views (Image) from the Continuous Troubleshooter to a folder that the user does not have write access to causes the Troubleshooter to crash.

562498

Realtime Action Objects cannot be deployed if the Runtime Manager and Runtime Services are running in different accounts.

567568

Discrete and Batch Troubleshooter may close unexpectedly when exporting the classification model multiple times.

569392

The Secure Deployment Guide information on how to change and restrict the CSense Action Objects & Services has missing information.

569836

When performing an advanced installation and using a remote SQL Server, Test Connections to the Data Server passes but selecting next may incorrectly display a Data Server version mismatch error.

  

CSense 2024- Last updated: June 20,2025