Known Issues

Defect # Area Description

DE180314

Continuous Troubleshooter

Simulating different P and I settings fails for Sampling Times other than 1 sec.

DE180334

Installer

During advanced Installation of the Application Server the permissions for users are not set up correctly.

DE180661

Process+ Action Objects

Process+ Ad hoc Action Objects do not stop execution after completing execution for the specified data window.

DE171768

General

Some resources and screens may not be translated for international versions of CSense.

DE172360

Continuous Troubleshooter

When exporting data from the CSense Troubleshooter the decimal separator is always a comma regardless of the regional settings specified for the target machine.

DE172450 

Continuous Troubleshooter

Continuous Troubleshooter projects that contain system identification items cannot be used between different supported languages.

DE176485

Continuous Troubleshooter

Numerical columns may not sort correctly in Continuous Troubleshooter.

DE177243

OPC Client Source Block

The OPC Client Source does not work as expected when using async to connect to a CSense OPC Server while deployed in the Action Object Manager.

DE177535

Template Blocks

Blueprint properties are not included in the resulting blueprint when expanding a template blueprint from within the Architect.

DE177960

Historian Source Block

Some users have reported that browsing tags using the Historian Source block in the Architect or Process+ deployment screen in the Action Object Manager is not performant.

DE13340

Blueprints

The Lookup Table 2D block output field values may change without updating timestamps.

DE19811

Architect

Architect may stop and exit unexpectedly when converting a field to double in the Text Source block property page.

DE69230

Connectivity

When OPC Client Source and Sink blocks reconnect to a CSense OPC Server both client and server Action Objects may go into an error state.

DE131928

Analytic Repository

Executing a block in the Architect that was previously published to the Analytic Repository with statefull execution enabled may cause the Architect to terminate unexpectedly under certain conditions.

DE135748

Blueprints

Under specific conditions the Historian Source Block may produce incorrect Field timestamps when the block is configured to execute in real-time mode.

DE136488

Connectivity

The Optimized DB Sink block fails to reconnect to SQL Server on connection failures.

DE136862

Blueprints

The template block 'Full Runnability Check' and 'Expansion' fails if the template contains an output port block that was configured to be locked but not all the output fields were used.

DE137735

Connectivity

Architect hangs when connecting to Oracle with a non SYSDBA user using the Tabular blocks.

DE137907

Connectivity

The Optimized DB Source block is unable to retrieve data from Oracle.

DE137915

Data Recipes

Under specific conditions when opening a previously saved Troubleshooter project open Data Preparation views may continue to display a ""Loading"" message without recovering.

DE137921

Connectivity

Oracle Oledb driver fails when used with the Database Table Import operation.

DE148898

Blueprints

When a blueprint contains a feedback loop before model inputs the offline trainer fails to train the model and reports and error.

DE149486

MPC

When removing MVs from the configuration in the MPC Editor the Model section information is lost.

DE153270

Decision Tree

Ruler behavior is inconsistent when using the ruler on a leave node of the Decision tree in the Discrete and Batch Troubleshooter.

DE153272

Architect

Setting a custom scale on a Probe Group in the Architect displays a message indicating that the configured value is not a valid number.

DE154488

Blueprints

Text Sink roll-over produces too many files when reading data sampled at 1 second intervals.

DE155300

Regional

Changing the Date Time format of the machine to English on a Japanese OS may cause some property lists to show corrupted text.

DE155986

Blueprints

The PLS Analysis block does not produce VC values for some input fields when running over a moving window.

DE156065

Blueprints

The PCA Block returns inconsistent timestamps on output fields when using a trigger field.

DE156861

Continuous Troubleshooter

Scenario Analysis sliders cannot be moved in Continuous Troubleshooter.

DE157723

Blueprints

The Feedback block property page filters may cause exceptions to be shown when filtering the list of feedback fields for Timestamps or Initial Quality.

DE158341

Continuous Troubleshooter

Exporting a Data file from the Continuous Troubleshooter does not use the system configured date separator for exported timestamps.

DE161013

Continuous Troubleshooter

Under specific conditions the Reconfigure operation may be incorrectly enabled for some datasets when a dataset is loaded in Step 2 of the Continuous Troubleshooter.

DE162590

Discrete & Batch Troubleshooter

The Discrete and Batch Troubleshooter may display empty data when plotting string vs string scatter plots.

DE159585

Data Recipes

The Data Preparation Merge operations fail when importing fields with matching names and differing cases.

DE164313

Architect

Overloads are shown when executing a blueprint in the Architect in Playback mode when the sampling period is set to Raw by time for a Historian source block.

DE164315

Architect

Under specific conditions when executing a blueprint in Playback mode in the Architect a user may be unable to Stop execution.

DE164565

MPC

Under certain conditions the MPC block execution may produce a division error when using slope control.

DE164889

Data Recipes

When transposing field names that has special characters using the Transpose operation in a data recipe the names are not auto corrected(not replaced with underscore).

DE165341

System Identification

System Identification in the Continuous Troubleshooter may produce incorrect models when performed on input data that contains a change in CV with no measured change in PV or when a step change in CV results in a step change in PV at the same timestamp.

DE165552

Real-time Action Objects

After completing an upgrade from a previous version of CSense real-time Action Objects that were running prior to starting the upgrade may not automatically start up after installation. Restarting the CSense Runtime Service or the machine will restart all previously deployed Action Objects.

  

CSense 8.5 SP1- Last updated: July 09,2025