Fixed Defects

Defect # Area Description

DE181007

Process+

Resolved an issue on the Loop Shift Performance Report where the shift performance table did not display data for all shifts.

DE181006, ,Process+,Resolved an issue on the Loop Shift Performance Report that showed incorrect shift data in the shift performance table when

DE181006

Process+

Resolved an issue on the Loop Shift Performance Report that showed incorrect shift data in the shift performance table when a shift was selected on the report filters.

DE180602

Process+

The default sort order for the Fleet Performance report has been updated to correctly sort on Average Performance Index showing the worst performing loops first.

DE177516

Process+

Resolved an issue where the Percentage Control On Process+ KPI was incorrectly calculated. This KPI now correctly calculates the percentage of the reporting period where data was good quality and the control mode was either auto or cascade.

DE175589

Process+

Resolved an issue where the Limits Exceeded KPI for a Process+ control loop was not calculated correctly when the limits were defined as a decimal value in regions that specify a symbol other than a comma ("") for the decimal separator.

DE180156

Process+

Resolved an issue where loops could not be deployed when limits were specified as zero ("0") in the loop definitions file provided during Process+ Action Object deployment.

DE177249 DE180092

Process+

Updated several documentation inaccuracies in the online help documentation for Process+.

DE166170  

Python Module Manager

Updated the Python Module Manager to include several stability enhancements enhanced user feedback more reliable backup and restore capabilities and significant updates to the general user experience.

DE176404  

Rate of Change Block

Resolved an issue where the Rate of Change block could terminate unexpectedly when using parameter fields from parameter ports.

DE172256  

Action Object Manager

Updated the Action Object Manager root screen to now display the correct number of deployed action objects and to provide accurate execution status for action objects listed.

DE177258              

Architect

Resolved an issue where some users would see duplicate block entries on the Architect palette after performing a version upgrade of CSense.

DE179086

Security

Updated the version of OpenSSL used by the OPC UA component in CSense to resolve an identified security vulnerability.

DE166782

Security

Updated the version of OpenSSL used by the OPC UA component in CSense to resolve an identified security vulnerability.

DE161344

Security

Updated the version of OpenSSL used by the OPC UA component in CSense to resolve an identified security vulnerability.

DE161343            

Security

Updated the version of LibXML used by the OPC UA component in CSense to resolve an identified security vulnerability.

 

 

  

CSense 8.5 SP1- Last updated: July 09,2025