About this task
An enumerated data set provides an
enhanced way of displaying data. It enables you to retrieve numeric data as string state
values. You can use the string values in reports, charts, etc.An enumerated set
contains several states. A state is the number-string value pair in a set. It
contains a set of numeric values and their corresponding string values. You can
define an enumerated set for a single value or a range of values. These state values
are defined for data states stored in Data Archiver. Data is retrieved using the
value of the state. You have to define state values within a set to assign
enumerated values.
Table 1. Example of a Single-Value Enumerated Set
State Name |
State Value |
Manual |
0 |
Automatic |
1 |
Table 2. Example of a Range-of-Values Enumerated Set:
State Name |
State Value |
ON |
0 to 100 |
OFF |
101 to 200 |
State names can be duplicated. If duplicated states exist, take
precautions to avoid unpredictable results. For example, a tag is associated with an
enumerated set defined as follows.
State Name |
State Value |
0 |
Open |
1 |
Close |
2 |
Close |
2 |
Open |
The server will return unpredictable results due to the State Name
duplication for an input of 2.Note: You cannot assign an enumerated set to an array tag.