Tags with Sequential Values
In addition to generating random values, the Simulation collector generates sequential values. The following table provides a list of tags for
which the collector generates sequential values. All the tags have a range of 0 to
1000.
Tags | Description |
---|---|
Constant | Maintains a constant value. |
Constant_1%Noise | Same as Constant, but produces 1% random noise. |
Constant_5%Noise | Same as Constant, but produces 5% random noise. |
Constant_20%Noise | Same as Constant, but produces 20% random noise. |
Ramp | Steadily increases value every polling period to create a smooth upward trend. |
Ramp_1%Noise | Same as the Ramp tag, but produces 1% random noise. |
Ramp_5%Noise | Same as Ramp tag, but produces 5% random noise. |
Ramp_20%Noise | Same as Ramp tag, but produces 20% random noise. |
Sin | Produces a Sine wave centered on a value of 500. |
Sin_1%Noise | Same as Sine tag, but produces 1% random noise. |
Sin_5%Noise | Same as Sine tag but produces 5% random noise. |
Sin_20%Noise | Same as Sine tag but produces 20% random noise. |
Step | Produces a step trend centered on a value of 500. |
Step_1%Noise | Same as Step tag, but produces 1% noise. |
Step_5%Noise | Same as Step tag, but produces 5% noise. |
Step_20%Noise | Same as Step tag, but produces 20% noise. |