Name |
String |
Enter the name of the tag. A value is required and must be unique. |
LocalName |
String |
Enter a unique identifier for the tag. A value is required and
must be unique. |
RemoteName |
String |
Enter the name of the tag that you want to use after it is imported to Historian. A value is required. |
ServiceName |
String |
Enter the service name used to connect to the eDNA server. You can enter multiple values separated by commas. A value is required. |
DataType |
String |
Enter the data type of the tag. A value is required. |
RemoteNameDesc |
String |
Enter the description of the remote name. A value is required. |
RemoteNameSpare4 |
String |
Enter the longID or extendedID of the tag. A value is required. |
RemoteNameSpare5 |
String |
Enter a description for the value in the RemoteNameSpare4 parameter. A value is required. |
RemoteNameEnggUnits |
String |
Enter the engineering units of the tag values. A value is required. |
TagName |
String |
Specify whether you want to use the extended ID or the long ID in the tag name. |