Export Tags as a CSV File

About this task

This topic describes how to export tags as a CSV file. You can export tags from Configuration Hub as a CSV file and add/modify tags in bulk and then import them. You can also import the CSV file that was exported using Excel Add-in.
Note: Similarly, you can also export enumerated sets, and user-defined types from the Manage Enumerated Sets and Manage User-Defined Types windows.

Procedure

  1. Access Configuration Hub.
  2. In the NAVIGATION section, under the Configuration Hub plugin for Historian, select Tags.
    A list of all the tags appears, displaying the corresponding details.
  3. Select and then select any one of the following options:
    Option Description
    Download CSV of this View Select this option if you want to download the selected tags and their corresponding details as listed in the tags grid.
    Download CSV with Tag Details Select this option if you want to download the selected tags and all their details, including configurations, from the DETAILS section.
    Note: Irrespective of the number of tags you select, all the available tags will be exported.
  4. Enter a name for the file and save it in a location as needed.